Zettler MZX Technology detection technology delivers early, reliable detection of all fire types, whilst remaining immune to most sources of false and unwanted alarms such as steam, insect infestation, and dirt build up.
Using some of the most powerful fire algorithms in the world, we can proactively determine when a device is going out of specification due to dirt build up and report that a service change is necessary. All devices have their own unique address which allows the control panel to inform building managers exactly where the seat of any event or incident is whether a real fire or an unlikely fault.
CO detection has proven to react so quickly to slow, smoldering fires (typically found in sleeping accommodation during quiet hours), that lives can be saved by issuing an early alarm notification to the presence of fire. This is a critical benefit for all sleeping risks, particularly in care homes where elderly and vulnerable persons are present.
Additional Benefits:
In large commercial buildings there are often multiple tenants occupying the space for different activities, including office space, call centres, canteens, small shops, and gyms. It is a challenge to find detection solutions that can satisfy the need of a multi-use building and help you limit unwanted false alarms.
Generation 6, 850PC Multi Sensor Detectors can help you overcome this problem. The Multi Sensor Detector has six detection modes, and employs three detection channels; heat, smoke, and combustion gas (carbon monoxide).