By using the most flexible wiring topography of any fire alarm system on the market, we offer architects and designers maximum coverage for minimum installation costs. The innovative Reflective Sound and Light Monitoring capability allows every device to self-test its sound pressure and lux outputs, and deliver a report at the panel on whether the unit has passed or failed the weekly test. This provides users with an audit trail to prove that not only have they discharged their responsibilities under current British Standards, but can also prove that each unit is working optimally.
Additional Benefits: