Ensuring fire and life safety during the COVID-19 pandemic
The COVID-19 crisis has resulted in an increased demand for alternate care sites, which has in turn led to several spaces being restructured and repurposed. However, fire safety regulations must be kept in mind while creating these temporary spaces to ensure that the life safety code is adhered to.
Johnson Controls offers solutions to help this transition happen smoothly and safely. We have fire alarms, sprinklers and suppression systems to be installed in these facilities. We also keep in mind that these systems must be delivered quickly due to the urgent nature of these emergency room requirements. Read this document to find out how our expertise and workforce can help get these care sites ready for patients as quickly as possible.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)