- Home
- Stanford University - Stanford, USA
Stanford University - Stanford, USA
October 24, 2023
About Stanford University
Stanford Energy System Innovations (SESI) project represents a transformation of university energy supply from a 100% fossil-fuel-based combined heat and power plant to grid-sourced electricity and a more efficient electric heat recovery system.
Challenges
- Stanford University sought to radically reduce its
energy, fossil fuels, and water consumption. - They needed to replace an end-of-life gas-fired
trigeneration plant.
Solutions
- Johnson Controls OpenBlue technologies deployed to deliver reduced energy and water use in the central plant
- Key features of the CHC system include:
- Large heat recovery chillers (heat pumps)
- Replacing steam production and distribution with hot water
- Both hot and cold water thermal energy storage
- Advanced “model predictive control” energy management software
- Large heat recovery chillers (heat pumps)
Results
- Increased system efficiency with 6% more heat recovery
- 17% reduction in peak energy demand - 7.3 MW (35.9 MW vs 43.2MW)
- This combined with the energy use savings translated to ~$500,000 per year (10%) in cost savings vs highly efficient, modern plant baseline
- Reduced campus greenhouse gas emissions by 68% (and growing)
- Reduced domestic water use by an additional 15%
- Saved $459 million over Business as usual case over next 35 years
Related Items
Healthy Buildings
Johnson Controls Healthy Buildings generate returns while creating healthy, sustainable environments that drive occupant well-being.
OpenBlue
Applying data from both inside buildings and beyond, our customers can now manage operations systemically.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)